Wolfspeed Commercially Introduces Transparent Silicon Carbide Technology for Augmented Reality and Quantum Computing

October 29, 2026

Proprietary TSiC™ technology enables new possibilities in advanced optical applications and next-generation computing

Wolfspeed, Inc. (NYSE: WOLF), a global leader in silicon carbide (SiC) technology, today announced the commercial introduction of its proprietary transparent silicon carbide (TSiC™) technology expanding the potential of silicon carbide to enable next-generation augmented reality (AR), quantum computing and advanced optical applications.

Wolfspeed TSiC™ technology is commercially available and will support optical applications such as AR/VR and quantum computing.

Wolfspeed TSiC™ technology is commercially available and will support optical applications such as AR/VR and quantum computing.

Wolfspeed builds on more than 35 years of silicon carbide innovation, including its pioneering work in LED technology and extensive experience manufacturing high-purity semi-insulating (HPSI) wafers. Wolfspeed’s optical-grade TSiC™ substrates are engineered for exceptionally low optical absorption and superior wafer flatness. Silicon carbide’s high refractive index, low birefringence, hardness and thermal conductivity make it a promising material for next-generation AR waveguides, supporting wider fields of view, improved image quality and more compact wearable devices.

Beyond AR, TSiC™ technology offers significant potential in quantum computing, with the ability to host quantum bits (qubits), preserve their quantum states and transmit quantum information through light—all within a single silicon carbide crystal. Unlike many alternative materials, silicon carbide can support all these functions.

“Wolfspeed’s leadership in silicon carbide innovation extends well beyond traditional semiconductor applications,” said Katrin Feurle, Vice President, Beyond Power at Wolfspeed. “Our proprietary TSiC™ technology and extensive intellectual property portfolio position us to help enable breakthroughs in augmented reality, quantum computing and other emerging markets, reinforcing the versatility and transformative potential of silicon carbide.”

"For years, the dream of truly immersive, all-day augmented reality glasses has run up against the hard limits of optical materials — you simply couldn't get a wide field of view, high image quality, and a lightweight, wearable form factor all at once," said Barry Silverstein, a display systems and optics industry expert at the University of Rochester and former Chief Technology Officer and Senior Director of Optics and Display Products at Meta Reality Labs. "Silicon carbide changes that equation. Its exceptionally high refractive index lets a single-layer waveguide do the work that previously took stacked optics, which is the kind of step-change the industry needs to move AR from a novelty into everyday eyewear. Wolfspeed's work on optical-grade TSiC™ technology is exactly the type of materials innovation that can finally unlock that potential.”

Wolfspeed’s technology is supported by a robust intellectual property portfolio, securing our technology advances with a strong intellectual property position. The company continues advancing its 200 mm optical-grade substrates while developing 300 mm TSiC™ technology to support future market requirements.

More information on TSiC™ technology, including requests for samples, is available here.

About Wolfspeed, Inc.

Wolfspeed (NYSE: WOLF) leads the market in the worldwide adoption of silicon carbide technologies that power the world’s most disruptive innovations. As the pioneers of silicon carbide, and creators of the most advanced semiconductor technology on earth, we are committed to powering a better world for everyone. Through silicon carbide material, Power Modules, Discrete Power Devices and Power Die Products targeted for various applications, we will bring you The Power to Make It Real™. Learn more at wolfspeed.com.

Wolfspeed® is a registered trademark and TSiC™ and The Power to Make It Real™ are trademarks of Wolfspeed, Inc.

Forward-Looking Statements

This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause Wolfspeed’s actual results to differ materially from those indicated in the forward-looking statements. Forward-looking statements by their nature address matters that are, to different degrees, uncertain, such as statements about Wolfspeed’s strategic plans, priorities, growth opportunities, and ability to achieve profitability. Actual results could differ materially due to factors detailed in Wolfspeed’s filings with the U.S. Securities and Exchange Commission (“SEC”), including its most recent Annual Report on Form 10-K and subsequent SEC filings. These forward-looking statements represent Wolfspeed’s judgment as of the date of this release. Except as required under U.S. federal securities laws, Wolfspeed disclaims any intent or obligation to update any forward-looking statements after the date of this release.

Media Relations:
media@wolfspeed.com

Investor Relations:
investorrelations@wolfspeed.com

Source: Wolfspeed, Inc.