Wolfspeed Introduces Industry's First Commercially Available 10,000 V Silicon Carbide Power MOSFET

March 5, 2026

Revolutionary 10 kV SiC Technology Delivers Game-Changing Solution for Grid Modernization, Industrial Electrification and AI Data Center Infrastructure

Wolfspeed, Inc., a global leader in silicon carbide (SiC) technology, today announced the industry's first commercially available 10 kV SiC power MOSFET. This milestone marks a defining moment in the industry — unlocking architectural freedom, delivering unprecedented system durability, and advancing access to reliable and sustainable power for the world's most demanding applications. This groundbreaking advancement challenges conventions in power conversion technology, delivering a transformative solution to modernize the grid and critical power infrastructure, to accelerate industrial electrification, and to unleash the potential for AI data center growth.

Wolfspeed's 10 kV Bare Die MOSFET

Wolfspeed's 10 kV Bare Die MOSFET

“This represents a historic leap in power electronics that will reshape how the world generates, distributes, and uses energy, unlocking the potential for modernization and more efficient power conversion," said Dr. Subhashish Bhattacharya, Duke Energy Distinguished Professor at North Carolina State University. "The timing of Wolfspeed's commercialization could not be better. The world is racing to connect AI data centers to the grid, and this will be the enabling technology for future generations of solid-state transformers at that critical grid interface.”

Read how this enables grid modernization in this article, “Answering the Call: Powering AI with Reliable Silicon Carbide-Based Solid-State Transformers”.

Unparalleled Reliability for Power Critical Applications

The 10 kV SiC MOSFET sets a new standard for durability and performance, with intrinsic time-dependent dielectric breakdown (TDDB) lifetime analysis predicting 158,000 years of operation at continuous 20 V gate bias voltage. As the first in the industry to solve bipolar degradation of 10 kV SiC MOSFETs, the device maintains reliable performance including body diode usage — essential for mid-voltage UPS systems, wind power, and solid-state transformer applications.

Architectural Freedom: Simplified Systems, Lower Cost of Ownership

The availability of SiC technology at 10 kV enables design flexibility that was not possible before, delivering a step function improvement in system’s size, weight, reliability, and cost of ownership.

  • Reduce system cost by approximately 30%: Using 10 kV SiC allows simpler system architectures consolidating multi-cell designs into fewer cells and downsizing three-level inverters to a two-level topology
  • Improve power density by more than 300%: Increasing switching frequencies from 600 Hz to 10,000 Hz simplifies control and gate drive circuitry, while also shrinking magnetics
  • Reduce system-level thermal requirements by up to 50%: Achieving 99% conversion efficiency enables simpler and more efficient thermal management compared to silicon IGBT-based systems

Realizing Pulsed-Power Potential: Enabling Next-Generation Applications

With a faster rise time of less than 10 nanoseconds, the new technology enables the replacement of conventional mechanical spark-gap switches — which degrade over time due to high-current, extremely high-temperature arcing that drives up maintenance costs and total cost of ownership — with SiC MOSFET-based solid-state switches. These solid-state devices eliminate arcing, enable efficient energy transfer, and improve timing precision of pulsed power transfer, while also reducing size and system complexity for high-performance pulsed-power applications including geothermal power, power generation for AI data centers, semiconductor plasma etching, and sustainable fertilizer production.

“This milestone is a culmination of nearly 30 years of vertically integrated crystal growth, thick epitaxy, and high voltage device manufacturing excellence,” said Dr. Cengiz Balkas, Wolfspeed chief business officer. “The commercialization of 10 kV MOSFETs enables our customers who have been prototyping at this voltage to transition their designs to production, accelerating time to market. We're not just ushering in a new era for high-voltage SiC - we're making it real.”

The 10 kV CPM3-10000-0300A SiC MOSFET die is available now for customer sampling and qualification.

About Wolfspeed

Wolfspeed (NYSE: WOLF) leads the market in the worldwide adoption of silicon carbide technologies. As the pioneers of silicon carbide, power modules and devices for a broad range of applications, the company brings you The Power to Make It Real.™ Learn more at wolfspeed.com.

Wolfspeed™ and The Power to Make it Real™ are registered trademarks of Wolfspeed, Inc.

Tyler Gronbach
Wolfspeed, Inc.
Vice President of External Affairs
Phone: 919-407-4820
investorrelations@wolfspeed.com

Source: Wolfspeed, Inc.